World’s 1st Grooved Mechanical Piping System for Saturated Steam Launched

Style 870 Coupling

World’s 1st Grooved Mechanical Piping System for Saturated Steam Launched

Posted on October 26, 2015

Victaulic, the world’s leading manufacturer of mechanical pipe joining systems, has developed the world’s first grooved piping system for saturated steam and condensate piping. Designed for use on commercial and industrial steam applications, the system features the Style 870 rigid coupling, a full line of fittings, and pipe preparation tool roll sets to process the new OGS-200 groove profile. The Victaulic grooved steam system eliminates the need to weld steam piping with pressures up to 150 psi (1,034 kPa) and temperatures up to 366 degrees Fahrenheit (186 degrees Celsius). Victaulic steam couplings and fittings ease installation and maintenance, compress the construction schedule, reduce downtime, and maintain a safer, more productive worksite.

“Engineers have long relied on the superior performance and design flexibility of Victaulic systems, while contractors depend on the total installed cost and time savings. We’re pleased to bring these benefits to steam systems for the first time,” said Kurt Gobreski, director of valves & large diameter systems with Victaulic. “This tremendous technological advance allows those who design, install and maintain steam systems to experience the absolute confidence that comes with specifying Victaulic.”

Joining steam piping with grooved couplings enables faster, easier installation than welding, threading and flanging. Pipe is joined by positioning the coupling seal and housing segments on the pipe ends and tightening the bolts and nuts to the specified torque requirement. Installation is completed up to five times faster than other joining methods.

With a union at every joint, the Victaulic piping system for saturated steam enables quick, simple maintenance, reducing downtime. The couplings simplify access to system components and ease pipe replacement and system expansion. Unlike flanged joints, Victaulic Style 870 couplings last the life of the system without regular maintenance. The couplings can also be used as a maintenance solution for existing steam piping, enabling leaks to be fixed quickly and inexpensively.

Assembling grooved couplings does not require heat or flame nor does it produce fumes, eliminating hazards to personnel and property during installation and maintenance. Hot works permits, fire watches, confined space welding procedures and X-ray inspection of joints are not required. Furthermore, the joining process mitigates environmental factors such as inclement weather conditions that complicate welding.

Victaulic steam system components are designed in accordance with the ASME Boiler and Pressure Vessel Code, as well as ASME B31.1, ASME B31.3 and ASME B31.9. Canadian Registration Numbers (CRN) are available for couplings and fittings upon request. The Victaulic Style 870 coupling and steam fittings—including elbows, tees, reducers, flange adapter nipples and caps—are available in 2- to 8-inch sizes (50 to 200 millimeters). Roll sets, which process OGS-200 grooves into Schedule 40 and 80 carbon steel pipe, are available for Victaulic VE272, VE416 and VE460 roll groovers.

For more information about the Victaulic piping system for saturated steam, visit http://www.victaulicsteam.com.

About Victaulic

Since 1919, Victaulic has been the originator and world’s leading producer of mechanical pipe joining solutions. Used in the most demanding markets, Victaulic innovative piping technologies and services put people to work faster while increasing safety, ensuring reliability and maximizing efficiency. The company has 12 manufacturing facilities and 31 branches worldwide with 3,600 employees who speak 43 languages across the globe. With over 1,900 global patents, Victaulic solutions are at work in more than 140 countries across diverse business lines including oil and gas, chemical, mining, power generation, water and wastewater treatment, military and marine, as well as commercial building and fire protection.

Related posts

Victaulic StrengThin Piping System

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

This innovative piping system solution allows for faster pipe fabrication & field installation, improves safety & reduces project costs.

Victaulic Booth at the AHR Expo

Victaulic Attends the AHR Expo with New Products & Technologies

Learn about our new grooved pipe joining products & technologies at the 2015 AHR Expo in Chicago.

Victaulic Compact Hydronic Balancing Valve

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

The TA Series 7CP advances hydronic balancing with its compact size & ability to engineer high performance systems.