Victaulic in Asia Pacific Unit 06-10, 3A/F, A Mansion, No. 291 Fumin RoadShanghai, China 200031Phone: +86 21 6170 1222Fax: +86 21 6170 1221E-mail: vicap@victaulic.com Victaulic is the originator and developer of the grooved piping method for rapidly joining pipes. For more than 80 years, Victaulic has been a leading manufacturer for HVAC/PHA, Plant Piping, Fire Protection and other specialized building service piping applications. Other uses of the Victaulic system include mining, maritime, oilfield, OEM, and industrial applications, such as chemical, pulp and paper, food, automotive, textiles, iron and steel, and power. Piping products for joining steel, ductile iron, HDPE, PVC, stainless steel, copper, aluminum and other types of pipe materials are also available from Victaulic. Customers located in Asia and Australia are serviced through the Customer Care Center in Shanghai.
Victaulic in Asia Pacific Unit 06-10, 3A/F, A Mansion, No. 291 Fumin RoadShanghai, China 200031Phone: +86 21 6170 1222Fax: +86 21 6170 1221E-mail: vicap@victaulic.com
Victaulic in Asia Pacific
Victaulic is the originator and developer of the grooved piping method for rapidly joining pipes. For more than 80 years, Victaulic has been a leading manufacturer for HVAC/PHA, Plant Piping, Fire Protection and other specialized building service piping applications. Other uses of the Victaulic system include mining, maritime, oilfield, OEM, and industrial applications, such as chemical, pulp and paper, food, automotive, textiles, iron and steel, and power. Piping products for joining steel, ductile iron, HDPE, PVC, stainless steel, copper, aluminum and other types of pipe materials are also available from Victaulic. Customers located in Asia and Australia are serviced through the Customer Care Center in Shanghai.
Piping products for joining steel, ductile iron, HDPE, PVC, stainless steel, copper, aluminum and other types of pipe materials are also available from Victaulic.
Contact (English) Contacto (América Latina) Contatti (Italiano) Contactperson (Flemish) 联系地址 (Chinese) Contacto (Español) Contact (Français) Kontakt (Deutsch) Kontakt (Polski) 연락처 (Korea)