Construction Canada Showcases Victaulic’s Contribution to 2010 Olympics and the Vancouver Convention Centre
In the March 2010 “Green Issue,” Construction Canada profiled the main 2010 Winter Olympics facility, the Vancouver Convention Centre, and Victaulic’s role in the unique seawater system used for the heating and cooling systems. The revolutionary system pulls water from the harbor, which is then used to heat and cool the building. The use of Victaulic not only contributed to sustainability of the centre, but also helped reduce installation time so the facility was completed on schedule.
Construction Canada reaches 12,445 construction specification writers, architects, builders, engineers and designers. The publication strives to keep readers up to date on business, technology and legal changes within the construction industry.