myVictaulic.com | VictaulicCastings.com
Gasket Technology

 
Victaulic utilizes various in-house advanced testing procedures and equipment to evaluate the temperature-decomposition profile of material, compression and pressure tests, joint performance in service under
minimum and maximum conditions, and independent lab verification.
 
 
 
 
 
 
Research and development are a core focus at Victaulic. Recently, the Victaulic engineering team developed a clean EPDM compound that may reduce microbial growth in Reverse Osmosis (RO) systems.
 
Microbial growth in RO systems:
  • affects water quality 
  • accelerates membrane bio-fouling 
  • decreases system recovery rates 
  • increases facility costs and decreases productivity
Project engineers researched EPDM compounds with the objective to design a “clean” compound by eliminating all possible organic nutrients that might support microbial growth. 

Figure 1: Shows typical biomass sample scraped from a rubber plate.
TEST AND RESULTS:
Microbiological resistance of eight Victaulic gasket compounds labelled A through H and two commercially available gasket compounds X and Y, were evaluated using three quantitative methods: biomass volume (W270), mean dissolved oxygen difference (MDOD) and chemical oxygen demand (COD). Based on the results, the researchers identified ingredients that do not support microbial growth, and optimized
a new compound - Victaulic Trial G.

CONCLUSION:
An important step in reducing microbial fouling in RO systems is the careful selection of wetted system components including elastomeric materials. The proprietary Victaulic Trial G compound was specially reformulated with ingredients
that were identified as non-supportive of microbiological growth and performed up to 75 times better than commercially available potable water approved compounds.

Figure 2: Shows the amount of biomass formed per 800cm2 rubber specimen for 11 different EPDM compounds after the 12-week immersion. Similar results were also obtained with Mean Dissolved Oxygen Difference (MDOD) and Chemical Oxygen Demand (COD) methods.

For more information on Victaulic gaskets read submittal 05.01.