myVictaulic.com | VictaulicCastings.com
Grooved System Pressure Test

Style 31 coupling  cutaway
 
Victaulic Style 31 couplings for AWWA piping systems were pressure tested to 1500 psi/10350 kPa, which is 3 times the rated working pressure, for a period of 3 minutes on Class 53 pipe. There were no leaks.
 
In phase two of the test a 285 psi ductile iron flange on Class 53 pipe was pressurized to failure.
 
Condensed test video ( Approx. 1 minute in length)
 
Full test video (Approx. 8 minutes in length)