myVictaulic.com | VictaulicCastings.com

How Pressfit Works
The heart of the Pressfit system's design is its precisely molded, synthetic rubber O-ring gasket.
 
A secure, permanent leak-free joint results when the system's O-ring is compressed against the pipe, deforming the pocket holding the O-ring and sealing the fitting to the pipe's outer diameter.
 
  
1. O-Ring
Precisely molded gasket made of synthetic rubber in several application grades for a variety of wet and dry services.
2. O-Ring Pocket
Sized to contain the O-ring before assembly, the pocket is deformed around the O-ring during compression to fully surround the pipe for a leak-free seal.
3. Housing
Precision formed stainless steel construction incorporating the pipe stop and O-ring. Adapters are available for easy field make-up of fitting combinations to threaded components.
4. Pipe Stop
An internal pipe stop locates pipe position to ensure positive joining.
5. Insertion Mark
A witness mark on the pipe ensures visual verification that the full pipe has been inserted for proper installation.
6. Tool Indent
The Pressfit hand tool engages the entire circumference of the bead on the fitting housing to ensure a secure attachment of pipe to fitting.