myVictaulic.com | VictaulicCastings.com
Press Releases - North America
   
Victaulic Develops Clean EPDM Gasket That Helps Reduce Microbial Growth in Reverse Osmosis Systems
7/20/2010
Victaulic, the world's leading manufacturer of mechanical pipe joining systems, has developed a clean EPDM gasket compound that may reduce microbial growth in reverse osmosis (RO) systems...
Victaulic Unveils Coupling for Fiberglass-Reinforced Plastic Pipe
7/14/2010
Victaulic, the world's leading manufacturer of mechanical pipe joining systems, today introduced the Style 296A coupling for fiberglass-reinforced plastic (FRP) pipe...
New Seminar Series Gives Engineers and Owners the Keys to Unlocking Hydronic Balancing
4/16/2010
Victaulic, in partnership with TA, brings the TA Hydronic College to 12 cities across North America...
Victaulic to provide piping systems for four landmark buildings at Shanghai World Expo 2010
4/2/2010
Grooved pipe assembly supports green goals of the exhibition...
Victaulic Announces New Director of Marketing and Communications
1/25/2010
Eric Luftig brings 15 years of experience to his position leading Victaulic’s global marketing efforts...
Victaulic Couplings Demonstrate Earth-Shaking Results During Testing
1/25/2010
Victaulic put its products through extensive third-party testing and confirmed that Victaulic couplings maintain operational integrity of piping systems during seismic events....
Victaulic Updates its Exclusive Installation-Ready Line, Which Allows for Quick Installations of Piping Systems
1/25/2010
The line gives contractors, engineers and owners an unmatched competitive edge, cutting installation time in half and making installations safer....
Victaulic Updates its Installation-Ready Product Line with the Availability of the Style 107H QuickVic® Rigid Coupling
1/25/2010
The Style 107H offers enhanced pressure ratings, and proven installation-ready technology...
Victaulic Helps Vancouver Olympics Facilities Complete Construction on Time and Sustainably
1/22/2010
Victaulic has been installed on over 20 Olympic facilities since 1976...
Victaulic Introduces the Only Direct Groove Two-Piece Coupling for Large Diameter Piping Systems
11/5/2009
Two-piece coupling design makes it faster and easier to install, maintain and retrofit piping systems up to 60” in diameter. ...
1  2  3  4  5  6