myVictaulic.com | VictaulicCastings.com
Press Releases - North America
Victaulic to provide piping systems for four landmark buildings at Shanghai World Expo 2010


 
Beijing (April 2, 2010) – Victaulic, the world’s leading supplier of mechanical pipe joining systems, today announced that four major buildings at the Shanghai World Expo 2010 are using its piping systems for key building services. The Expo Center, the Expo Culture Center, the Expo Axis and the China Pavilion all rely on Victaulic piping systems for their HVAC (Heating Ventilation and Air Conditioning), fire services and water supply needs. 
 
Although not new to high-profile projects, Victaulic representative commented that the contracts  represent a major achievement for the company at one of the world’s highest profile events. More than 190 countries and an estimated 70 million people will attend the massive exhibition, which commences on 1 May in China’s largest city. 
 
“We are delighted to have been chosen to provide systems for these prestigious structures and for playing our part in this international exchange and communications event,” said Ms. Ying Cao, East China Region Sales Manager for Victaulic. “Each building will receive millions of visitors so it’s important that all building functions work smoothly and without fault. Being a six-month show, the core HVAC will face both the heat of summer and the cold of autumn but we remain confident that our piping systems will perform reliably.” 
 
The Victaulic grooved piping system was selected for its ease of installation with its grooved-end method of joining pipe being three to four times faster than similar welded or flanged pipes. The system is also notably greener with all Victaulic products made from natural and recycled resources -- an important consideration given the sustainable development messages of the exhibition. “Better City, Better Life” is the core theme of the exhibition. 
 
Grooved piping systems do not emit CO2 and other harmful gases during installation and maintenance and also do not need electricity during installation. Safety is also improved since no open flames are required as is the case for welded pipes.  
 
The main Expo Center will be used to receive foreign leaders and hold ceremonial activities such as the event opening. The center is a green and low-carbon building constructed in accordance with China's 3-Star Green Building and the American LEED Gold Building standards. A host of advanced technologies are incorporated, including solar panels, LED lighting and a river water-source heat pump, the goal being to achieve the highest levels of energy conservation and emissions reduction.
 
The Expo Culture Center is located by the riverside in the Huangpu District. During the Expo, it will be a cultural focal area for performing arts, exhibitions and entertainment. The irregular shape of the building is comparable to that of the “Bird’s Nest” building in Beijing. This provides unique visual enjoyment but also posed some difficulty when it came to the piping system installation. The internal pipelines of Expo Culture Center are very complicated.
 
The design and installation company made a 3D model beforehand and chose the Victaulic grooved piping system to accurately meet various design requirements of the building. The Victaulic system consists of coupling housings, two bolts and nuts and a gasket. Highly customizable, the solution provides both rigid and flexible couplings so the pipes can be installed at any angle and can meet the various bends and corners found in a building. 
 
The imposing China Pavilion, designed with the concept of the "Oriental Crown", embodies much of the best of Chinese culture and is one of the most striking at the Expo.
 
“Normally it takes around three years to construct a similar building. However it was assembled in just two years to meet the tight timelines. Grooved piping was ideal for the task given its speed of assembly,” said Ms. Cao. 
 
The Expo Axis is the main access and transport hub for the Expo and incorporates the world’s largest membrane roof. It is estimated that the Expo Axis would receive an average of 92,000 visitors per day when the show begins. Since it could become very crowded, fire safety is of paramount importance.
 
“The safety of products, the installation and maintenance safety, as well as the venue’s operational safety are all crucial to the choice of piping system for the Expo facilities. As a world-famous brand, Victaulic fire protection and HVAC products can satisfy the Expo’s requirement for reliability and safety, as well as energy and environmental conservation. In addition, its professional and timely service impressed us”, said Shenghui Li, General Manager of Shanghai Installation Engineering Company, Ltd, the contractor for the pipework.   
 
Victaulic’s fire protection products used in the buildings include FireLock V36 Series Dry Sprinklers, Series 705 Butterfly Valves, and the Series 769 FireLock NXT Deluge Valves. The FireLock V36 Series Dry Sprinklers are the only products in the industry that pass the stringent inspection of the Tianjin Fire Research Institute of Ministry of Public Security. The working pressure of the Series 705 Butterfly Valve is up to PN21. The Series 769 FireLock NXT Deluge Valve is easy to install and maintain, occupies a smaller footprint in the space than other valves and also is lighter in weight.
 
Aside from the World Expo, Victaulic’s grooved piping systems were previously used at the 2008 Summer Olympics in Beijing, including the main “Bird’s Nest” stadium, the National Aquatics Center (Water Cube) and National Grand Theater. They are also installed at the Shanghai Jinmao Tower, Shanghai World Financial Center and Taipei 101.
 
About Victaulic
Founded in 1925, Victaulic is the world’s leading producer of mechanical pipe joining systems. Headquartered in Easton, Pennsylvania, USA Victaulic has manufacturing and distribution facilities worldwide and employs more than 3,500 people. The company develops products for a full range of industrial, commercial and institutional piping system applications. For more information, please visit www.victaulic.com.