myVictaulic.com | VictaulicCastings.com
Press Releases - United Kingdom
Big and Bold with Victaulic Large Diameter Advanced Grooving System


 
Victaulic®, the world leading grooved pipe joining system manufacturer, is now able to offer UK installers a complete range of large diameter rigid and flexible couplings, fittings, valves and accessories - the Advanced Groove System (AGS).

The introduction of the Vic-Flange® Adapter and stainless steel rigid coupling to the AGS product line ensures that this large diameter product range offers users a total package solution for any HVAC and industrial process piping installation. Offering unprecedented performance and reliability thanks to an innovative patented design, AGS is now the company’s strongest pipe joining system for large diameter pipe.

Ideal for HVAC and industrial process piping applications, the Victaulic Advanced Groove System is available from 350mm – 600mm and is designed with performance, speed and ease of installation in mind. With a two-piece housing, requiring only two fixing bolts and a new wedge-shaped groove that delivers pressure ratings up to 350 psi (24 bar), the Advanced Groove System offers unprecedented assembly speed and reliability. In addition, the coupling also provides visual confirmation of correct assembly via a metal-to-metal bolt-pad design, ensuring ultimate product inspectability.

The addition of the Style W741 Vic-Flange Adapter, enables flanged components with ANSI CL. 125/150 bolt-hole patterns to be accommodated within a Victaulic grooved end installation. The Style W741 provides a rigid joint when used on pipe with AGS roll groove or cut groove dimensions and consequently does not allow linear or angular movement at the joint. The Style W741, rated up to 300 psi/2065 kPa, is available in sizes ranging from 350 – 600mm.

To complement the existing range, Victaulic has also added the Style W89 AGS Rigid Coupling, which is designed for use exclusively with stainless steel pipe Schedule S10 or higher. Developed for use with

HVAC and industrial applications to provide an inflexible joint, the Style W89 coupling greatly reduces linear and angular movement through the use of wedge-shaped coupling housing keys which fully engage the grooves to provide rigidity on valve connections and other points.

Available in sizes 350-600mm, and for pressures up to 300 psi/2065kPa, the Style W89 couplings are provided with plated bolts and nuts and FlushSeal® gasket Grade “E” EPDM for multiple uses. Grade “T” nitrile and Grade “L” silicone are also available. Dependent on gasket grade, the Style W89 couplings are suitable for various temperatures ranging from -30ºF/-34ºC to 350ºF/177ºC.

In addition to streamlining coupling assembly, the Victaulic Advanced Groove System also simplifies pipe-end preparation by using a unique single groove profile that is designed to eliminate the possibility of pipe-end flare. Specific AGS roll sets are used with existing Victaulic tools, the only tools on the market capable of grooving up to 1200mm. All Victaulic grooving tools are designed and manufactured by Victaulic.

Fred Matyiku, country manager, UK and Ireland, comments: “Our AGS family offers engineers and contractors a wide range of design and installation benefits that are superior to welding. Not only does the range extension mean that we can now offer flanged adaptors and rigid couplings for stainless steel applications, but it shows that we as a company are continually listening to our customers and developing products to make their lives easier. The more robust coupling housing and deeper, wider groove, offers stronger joint integrity and a continuous seal around the gasket, making AGS one of our most exciting product ranges.”

Victaulic, a privately held company headquartered in Easton, Pa., U.S.A., has manufacturing and distribution facilities worldwide and employs approximately 3,000 people. The company, and its subsidiaries, develops products for a full range of industrial, commercial and institutional piping systems.

For more information on the Victaulic product range or stockists, call Victaulic in the UK on 01438 741100 or visit www.victaulic.com
 
Contact:
Bonnie Turner/ All Patel, Publicasity
Tel: +44 (0) 1442 261199