myVictaulic.com | VictaulicCastings.com
Press Releases - United Kingdom
Victaulic Showcases the HEart of Fire Protection at IFE 07


 
Victaulic, the world leader in pipe joining system manufacture, is showcasing the heart of its fire protection technology at International Fire Expo 07 this year – its new range of FireLock NXT™ devices and FireLock EZ™ Style 009V of rigid couplings and fittings. Ideally suited to the UK market, the FireLock NXT range provides a simple solution for either wet or dry applications in one device and the FireLock EZ™ Style 009V will prove very popular with visitors, due to its pre-assembled, no-loose-parts approach to installation.

Developed following close consultation with designers, installers and facilities managers, the FireLock NXT line of dry, deluge, alternate and preaction devices for fire protection systems is quick and easy to fit and offers the smallest installation footprint in the industry.

FireLock NXT devices are LPCB approved and rated to 2065kPa/ 300 psi. They are available in sizes ranging from 40mm to 200mm. With an integral Victaulic-patented low-pressure actuator, FireLock NXT devices can be operated at lower pressures due to an eliminated air-to-water differential, ensuring faster water delivery to sprinkler systems. In addition, each valve has a pre-set air supervisory switch, speeding up the installation process and minimizing the potential for human error.

The Firelock NXT alternate valve takes wet and dry fire protection to the next level. Not only does it provide both wet and dry functionality in a single valve but also requires the adjustment of only three valves to drain and re-pressurize the system for warm or cold weather. For speedy installation, the valve (weighing as little as 43kg) can also be
shipped pre-trimmed with only the need for pressure gauge connection on arrival.

Based on feedback from fire protection contractors, the revolutionary FireLock EZ™ Style 009V rigid coupling is designed as a lightweight, installation-ready coupling with no loose parts. It is not necessary to disassemble the coupling for installation, shaving even more time off the already quick installation time of this mechanical grooved joint. Plus, the angled-bolt pad design enables pad-to-pad assembly without the need for a torque requirement, as well as providing visual confirmation of proper installation once fitted. The coupling carries listings and approvals from VdS, LPCB, UL and FM and is rated to 16 bar/1600kPa/232 psi. FireLock EZ™ Style 009V is available in nominal sizes 32mm – 100mm (1 ¼”-4”/actual OD 42.2mm 114.3mm).

Fred Matyiku, country manager, UK and Ireland, comments: “We have chosen IFE 07 to showcase Firelock NXT and EZ™ Style 009V, as they are central in terms of cost, time and maintenance benefits for any consultant involved in the design, installation or
management of a fire protection system. With the wet and dry functionality of the NXT devices meaning only one valve need be installed along with the built in speed of installation of the EZ™ Style 009V, we are expecting the ranges to be very popular across the UK, Ireland and Europe”.

For more information on the Victaulic product range or stockists, contact the Victaulic office in the UK on 01438 310 690, in Ireland on 0124 60219 or visit www.victaulic.com .
 
About Victaulic
Victaulic, a privately held company headquartered in Easton, Pa., U.S.A., has manufacturing and distribution facilities worldwide and employs approximately 3,000 people. The company, and its subsidiaries, develops products for a full range of industrial, commercial and institutional piping systems.
 
Contact:
Daniel Charcharos/ Ali Patel Publicasity
Tel: +44 (0) 1442 261199