MyVictaulic.com | VictaulicCastings.com
Testimonials
  
Greg Lee, President
DFW Fire Protection, Inc.
Dallas, Texas
 
“We were able to show the engineering team that by using Victaulic grooved products, they would get a consistent roll grooved piping system and Schedule 10 piping could be used instead of cut-grooved Schedule 40 pipe. The move to Schedule 10 led to an approximate 50% savings in pipe materials overall.”
 

 
Gary Burns, President
Poole & Kent an Emcor Company
Baltimore, Maryland
 
“Close coordination between Victaulic and Poole & Kent was necessary due to the tight confines within all mechanical rooms. To Victaulic’s credit, their attention to detail and sense of urgency to complete the drawing process resulted in a detailed drawing package that allowed [us] to seamlessly install multiple layers of piping within all mechanical spaces. The amount of detail on the Victaulic drawing packages helped [us] to manage our labor costs more efficiently.”
 

 
Joey Doxey, Production Manager
Hiller Systems
Chesapeake, Virginia
 
“In the valve room, the pre-assembled valves and Vic-Quick risers really made the difference with keeping up with the tight schedule and saved a good three days of labor.  Also, working in a freezer space, the pre-assembled couplings helped ensure that the gaskets stayed dry and did not get water inside the seal."
 
 

 
Mike Bridges, Project Director 
Galiford Try
London, United Kingdom
 
“We have been working with the All England Lawn Tennis Club (AELTC) for over 30 years on refurbishments at Wimbledon, however Centre Court is our biggest project to date.  It is our aim that all the pipework will be installed, tested and lagged before the winter, and we are well on our way to achieving this target thanks to partnerships such as the one we have with Victaulic.”
 
 

 
Basheer Massad, Project Manager
BK Gulf
Dubai, UAE
 
“Being able to demonstrate to [the owner] on paper the inherent savings to cost as well as speed of the Victaulic system made my life a lot less stressful. I was able to order the product well in advance and time its arrival onsite to coincide with each stage of the job.”
 
 

 
Jules Petrinec
Paul Ellard-Willson & Associates
Toronto, Canada
 
“The grooved piping method is the most versatile, reliable and economical system available for joining pipes on a project of this nature. It’s up to three times faster than welding, easier than threading or flanging, and offers the combination of mechanical advantages required for a tower installation.”
 

 
Bulent Barutcu, Chief Mechanical Engineer
MEP Construct International
Romania
 
“It was recommended that we use a new ‘installation ready’ fire protection coupling from Victaulic—the Firelock EZ™ Style 009V. The results were significant: We were able to reduce man-hours on site by 35% and meet the tighter building deadlines.”
 

   
Rusty Gravitt, President
Gainesville Mechanical Inc.
Georgia, USA
 
“In estimating project profitability, we know historically we can produce 75% more revenue per man-hour using Victaulic systems—primarily because the grooved and Pressfit solutions are so much faster to install. We can use fewer men per project using Victaulic than when using a traditional welding or thread and couple system. Victaulic allows us to be more accurate in the bid process because their system is much more predictable.”