Victaulic Products Featured in AgriBio Research Centre in Melbourne
The February 2012 issue of Engineers Australia featured an article about the AgriBio Research Centre in Melbourne, Australia. La Trobe University and the Victorian Department of Primary Industries will occupy the space once it is completed later this year. Located in the suburb of Bundoora, the $288 million centre began construction in May 2009 and will accommodate up to 400 staff and students. Contractor James Williams chose Victaulic mechanical pipe joining systems, couplings, valves and joints for chilled and condensed water, fire protection systems and hot water systems for the project. In addition, Williams utilized drawing services from Victaulic Construction Piping Services (CPS).
Engineers Australia is the monthly publication of Engineers Australia, a national engineering organization. With a circulation of 22,219, the publication covers topics including general engineering news, events, features and a monthly sustainability section.