Water21 Features the Victaulic Vic-Ball® Super Duplex Valve Series 726D
The February 2012 issue of Water21 featured an article describing the benefits of the Victaulic Vic-Ball Super Duplex Valve Series 726D. In addition to providing easier, faster and safer installation than flanged and butt-weld valves, it can tolerate pressures of up to 8,200 kPa (1,200 psi). Connected by the Victaulic Style 489DX rigid coupling, which is comprised of only 2 bolts to create a secure joint, field installation is very efficient for both high-pressure and low-pressure applications.
Water21 is the official publication of the International Water Association – a leading UK-based water sector professional organization that aims to improve worldwide water management services. The publication has a global circulation of 20,000.