Victaulic Showcases its Exclusive Installation-Ready Line and Advanced Groove System Line

24 May 2011
Press Releases
Victaulic Showcases its Exclusive Installation-Ready Line and Advanced Groove System Line

Victaulic, the world's leading manufacturer of mechanical pipe joining systems, will showcase its patented installation-ready product line and Advanced Groove System (AGS) product line at HVAC Brussels 2010. Both product lines give contractors, engineers and owners an unmatched competitive edge, cutting piping system installation time and making installations safer. Installation-ready technology is designed to address the industry’s need to compress project schedules and remain competitive. It is the fastest and safest pipe-joining method currently available. The installation-ready coupling installs up to ten times faster than other pipe- joining methods such as welding, brazing, soldering or flanging. Installation-ready couplings require fewer steps to install, resulting in consistently faster pipe joints, which allows contractors to optimize crew size and better manage their labour risk. Also on display will be the Victaulic patented Advanced Groove System (AGS), the strongest and most dependable mechanical piping joining system for 350-1525mm (14-60”) size piping systems. With a two-piece housing and a wedge-shaped groove that delivers pressure ratings up to 2,400 kPa/350 psi, depending on the pipe size and wall thickness, Victaulic AGS couplings offer exceptional assembly speed and reliability. Visitors stopping by the Victaulic stand B022 will also benefit from on-site roll-grooving demonstrations utilizing Victaulic roll-grooving tools. Victaulic has a strong reputation worldwide. “Once our customers have experienced the benefits of using the Victaulic pipe-joining method, they come back to us time and time again,” says Regional Manager, Benelux, Bart Vandedrinck. “Visit stand B022 to find out how we can help make your next project a success”. Press enquiries: Elaine Essery, VIPR T: +44 (0) 1229 716129 E: elaine@vipr.biz For more information about Victaulic products or distributors, visit www.victaulic.com or contact +32 93 81 1500. About Victaulic Founded in 1925, Victaulic is the world's leading producer of mechanical pipe joining systems. Headquartered in Pennsylvania, USA, Victaulic has manufacturing and distribution facilities worldwide and employs more than 3,500 people. The company develops products for a full range of industrial, commercial and institutional piping system applications. For more information, visit www.victaulic.com.