Downloads

CAD Files & Software

Vic Iso

Required Software: AutoCAD Release 2007 or Higher

Designed specifically for AutoCAD users, VIC ISO is a two-dimensional block library that was developed to assist in the creation of Victaulic isometric drawings. It includes block symbols representing the main product line. Each component includes various isoplane orientations (left, right or top view). A common insertion point has been designated in each block for ease of placement. Components are inserted using the AutoCAD Design Center. The border drawings that are supplied with VIC ISO can also be used in conjunction with the AutoCAD copy command in order to create Victaulic isometric drawings.