Events

Victaulic Events

SICUR - International Security Safety & Fire Exhibition

Victaulic reveals new fire protection products at SICUR.

Victaulic is displaying a wide range of couplings, fittings, valves, sprinklers and devices designed to enable fast, efficient, cost-effective fire protection installations at the Salón Internacional de la Seguridad, Hall 8 booth 8E06, from February 28th to March 2nd.

Amongst the highlights will be the opportunity to catch a glimpse of the new addition to the Victaulic FireLockEZ® Style 009H Rigid Coupling range, and see a demonstration of its fast, consistent installation with or without power tools.
Victaulic listened to contractors looking for an easy to install coupling with no loose parts. The 009H ships to the jobsite ready to install and offers the fastest installation time on the market.

Other products on show at SICUR in Hall 8 Booth 8E06 will include Aquaflex Stainless Steel Sprinkler Fittings and the LP-46 sprinkler range.

AquaFlex enables rapid sprinkler installation on suspended ceiling grids, utilizing a 1375kPa rated braided flexible hose and a unique, adjustable open-gate center bracket, allowing easy center-of-tile installation in seconds.
• The LP-46 large K-factor standard-response low pressure pendent and upright sprinklers are designed to control fires in single, double and multiple row rack storage units without the need for in-rack sprinklers and meet all the requirements for maximum storage room protection.

Also on display will be the robust and ever popular range of Victaulic FireLock devices.
The Victaulic FireLock devices have major advantages for the installer, maintainer and owner. Because the devices are so simple to install and maintain, end users can be confident that the system functions correctly to give them continuous, reliable protection.

Event Dates and Location

Back to Events