Victaulic Vic-Ball® Super Duplex Valve Series 726D Featured in Desalination & Water Reuse Quarterly
The February 2012 issue of Desalination & Water Reuse Quarterly featured an article describing the benefits of the Victaulic Vic-Ball Super Duplex Valve Series 726D. In addition to providing easier, faster and safer installation than flanged and butt-weld valves, it can tolerate pressures of up to 8,200 kPa (1,200 psi). Connected by the Victaulic Style 489DX rigid coupling, which is comprised of only 2 bolts to create a secure joint, field installation is very efficient for both high-pressure and low-pressure applications.
Desalination & Water Reuse (D&WR) Quarterly has been published by the International Desalination Association since 1991. The journal covers emerging technologies and global engineering aspects of desalination and water reuse, from municipal water supplies to industrial needs.
View the article online at the Desalination & Water Reuse Quarterly website.