Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Centre for Agribioscience

AgrioBio, Centre for AgriBioscience is a joint initiative of the Government of Victoria and La Trobe University. Located at La Trobe University’s main campus in Bundoora, Victoria, AgriBio will be one of Australia’s premier bioscience facilities, with a key emphasis on supporting and protecting Victoria’s AUD$11.8 billion agricultural sector by focusing on cutting-edge research to improve productivity, fight disease and reduce environmental impact.

HVAC contracting firm James L. Williams was hired to manage the design and installation of the building’s cooling system, under a very tight build schedule. To meet the deadline, the contracting firm chose to use Victaulic’s full mechanical pipe joining system for its ability to cut installation time by up to 30%. In addition, James L. Williams utilised Victaulic’s Construction Piping Services (CPS) drawing package to provide 3D system drawings and analysis of system requirements, and to calculate the required work hours and manpower for the project.

The building will have Victaulic couplings, valves and joints installed across its chilled water, condensed water, and heating hot water systems.

Search Terms: PS-HVAC.357, PSHVAC357, PS.HVAC.357, PS-HVAC-357

Download

English - pdf (118 KB)