Case Studies

Victaulic can be found in some of the most prestigious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Hospital Cártama

Hospital de Cártama is a 15.300 square meter hospital in Malaga, which, when completed, will cover the needs of about 100.000 people. To make the piping system installation more efficient, contractor Ferrovial – Instalaciones Villalba employed Victaulic products in the hot, cold and condensed water lines, mechanical rooms and connections to main equipment. Victaulic was also selected for use on the Fire Protection system. 

Victaulic's no flame pipe joining solutions were specified because they are the best solution for confined space installation. Victaulic grooved systems feature a lower profile when compared to flanged systems, and therefore, grooved piping systems were installed in closer proximity of each other making it possible to work in tight spaces at an extremely flexible and effective working pace. To improve on site efficiency and material handling the Victaulic Construction Piping Services (CPS) team developed sets of detailed isometric drawings to ease construction in the mechanical rooms. By employing Victaulic Bag and Tag services products arrived pre-packed for use where and when needed on the jobsite. 

By using Victaulic solutions, the installation was completed in fifty percent of the estimated time used for joining pipe using alternative methods such as welding. Installing Victaulic products not only resulted in time savings, which reduced the costs, but also enabled Ferrovial – Instalaciones Villalba to cope with confined space installations.

Download

English - pdf (470 KB)

Select Language