HVAC
Heating Water
Victaulic offers a complete line of grooved products for 1/2-60"/15-1525 mm cooling systems including couplings, fittings, valves and accessories.
Victaulic grooved mechanical pipe joining systems
- 45% less man-hours on average over welding
- Eliminate costly fire watch and hazardous fumes and flames
- Reduce material handling by 30-70%
Value Engineering from Victaulic
- Accommodate piping movement with less stress on components.
- Maintain operational integrity of piping systems during a seismic event.
- Dampen overall vibration amplitude by 80-90 per cent.
Brands
-
QuickVic®
More About QuickVic® -
Advanced Groove System (AGS)
More About Advanced Groove System (AGS)
Featured Products
Featured Case Studies
-
Venetian Casino Hotel – 23 Feb 2011
Casino projects require tremendous coordination and design flexibility to successfully complete construction under aggressive schedules.
More about this Case Study -
Alexandria Library – 23 Feb 2011
Protecting priceless national treasures required a piping system that offered unparalleled reliability. Victaulic products were specified and installed to provide that service.
More about this Case Study -
Reliant Stadium – 23 Feb 2011
Reliant Stadium is home of the Houston Texans and the Houston Rodeo in Houston, Texas. This domed facility has a retractable roof structure and 75,000 seats.
More about this Case Study -
Nile City Towers – 23 Feb 2011
Because of the height of the towers, the project pushed local design and installation limits. The Victaulic grooved pipe joining method was chosen as the total system provider for the project because of it's ability to accommodate the tight space constraints in the riser shafts which was a result of a small site footprint.
More about this Case Study -
Goetzman Energy Plant Palm Beach Atlantic University – 23 Feb 2011
By using Victaulic piping systems on this project, the mechanical contractor was able to reduce totaled installed costs, provide for noise and vibration attenuation and make the system easier to access, install and maintain.
More about this Case Study -
Fort Greely Power Plant – 23 Feb 2011
In late 2009, construction was completed on the make-up water system at the United States Army Fort Greely Power Plant in Delta Junction, Alaska.
More about this Case Study -
Weener Energie – 23 Feb 2011
Kraftwerk Steam Power Plant is located in Weener, Germany and is owned and operated by Weener Energie.
More about this Case Study -
GTAA Cogeneration Plant – 23 Feb 2011
The Greater Toronto Airport Authority’s new 117 MW co-generation facility for Toronto Pearson International Airport opened in December 2005 to serve the electricity needs of the airport while supplying steam for heating and cooling. The plant will also produce a substantial amount of clean power that will be sold back into the province’s grid.
More about this Case Study