Process Piping

Process Piping Overview

The Victaulic grooved piping method meets the harsh demands of a variety of industrial piping systems. With couplings rated to 1000 psi/6900kPa and products to handle both abrasive and non-abrasive systems, Victaulic total systems offer ease and speed of installation, coupled with a robust, innovative joining method.

  • ZeaChem Cellulosic Biofinery Facility
    ZeaChem Cellulosic Biofinery Facility

    ZeaChem will be one of the first cellulosic demonstration plants built in the United States. The plant will produce Ethanol, glacial acetic...

  • Hyundai Motor Manufacturing
    Hyundai Motor Manufacturing

    The Hyundai Motor Manufacturing Plant in Montgomery, Alabama chose to use galvanized Victaulic systems on the compressed air cooling water, chilled water...

  • Glaxo Smith Kline Pharmaceutical
    Glaxo Smith Kline Pharmaceutical

    When Glaxo Smith Kline Pharmaceutical decided to spend $100 million on the expansion of the vaccine additive manufacturing facility, they chose to use...

  • Biodiesel Line
    Biodiesel Line

    Biodiesel refers to a vegetable oil or animal fat-based diesel fuel consisting of long-chain alkyl esters. Biodiesel is typically made by chemically...

  • Caustic
    Caustic

    A corrosive substance is one that will destroy or irreversibly damage another surface or substance with which it comes into contact.

  • Chemical Treatment System
    Chemical Treatment System

    Chemicals may contain caustic or damaging elements which demand careful handling. Processing chemicals often require stainless steel piping systems to...

Victualic