Utility Piping
Utility Piping Overview
With total system solutions for a variety of piping system materials, as well as gasket grades to handle specific media, Victaulic has a solution for your utility piping system.
The ease and speed of installation not only saves time, money and worry during initial plant construction; but, with a union at every joint, Victaulic eases the burden of planned and unplanned maintenance, with no need for hazardous flames and fumes, firewatches or building evacuation.
-
ZeaChem Cellulosic Biofinery Facility
ZeaChem will be one of the first cellulosic demonstration plants built in the United States. The plant will produce Ethanol, glacial acetic...
-
Interface Industrial Expansion
When Interface Industrial was looking to expand its manufacturing facility, they were under a tight schedule. The increased capacity would translate to...
-
Nissan North America Headquarters
When Nissan North America requested the Victaulic grooved pipe joining method for the construction of its 10-story headquarters, the unique request was...
-
Air Piping
Victaulic grooved end technology helps to ease deck and wall penetration and reduce system downtime of your air piping system.
-
Cooling Water
Install up to 10 times faster than other pipe joining methods.
-
Bearing Lube Oil Feed Lines
Oil feed systems are used to lubricate mechanical equipment and processes.
-
QuickVic® Rigid Coupling - Style 107H
Installs twice as fast as standard grooved couplings.
-
Vic-300 MasterSeal™ Butterfly Valve - Series 761
Designed for pressures ranging from vacuum to 300 psi/2065 kPa
-
Vic-Press™ Coupling for Type 316 Sch. 10S - Style P507
Press-to-connect coupling for Schedule 10S pipe.