News
Victaulic News
1 Feb 2011
Benefits of Using Victaulic Advanced Groove System in Remote Areas Featured in Arab Water World
Arab Water World featured an article in February 2011 highlighting the advantages the Victaulic Advanced Grooved System (AGS) provides over other pipe joining systems.
Arab Water World featured an article in February 2011 highlighting the advantages the Victaulic Advanced Grooved System (AGS) provides over other pipe joining systems. Victaulic mechanical joints can be assembled in remote areas because they require no power tools, can withstand any type of weather condition, and do not require flame during construction—a hazard in especially dry areas. The superior strength and reliability of the AGS allow up to a 40-percent increase in end load carrying capabilities, making it well suited for carrying water.
Arab Water World reaches 24,000 water-related professionals, predominantly engineers, contractors, importers/exporters, distributors, manufacturers and suppliers. The publication is read mostly in the UAE and Saudi Arabia.