Case Studies

Victaulic can be found in some of the most prestigious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Data Center Tres Cantos

The refurbished data center of Spanish bank BBVA in Madrid houses 36000 sqm of installations, with a capacity of 16.000 Kw and nearly 2,000 km of fiber optics. For the second stage of the refurb, consultant Aguilera choose Victaulic products to join the data center’s cooling system.

Normally time-consuming to weld, large diameter 14”/350 mm pipe was joined using the Victaulic Advanced Grooved System (AGS). Featuring a two-piece design, AGS couplings secure with just two bolts for quick and easy installation and can be visually inspected to ensure proper installation. Other products installed included a range of Victaulic fittings and QuickVic™ Style 107H and Style 07 rigid couplings.

By using Victaulic pipe joining solutions, phase two of the project was completed in half the time as phase one, which was specified weld.

 

Search Terms: PS-HVAC.456, PS-HVAC-456, PS.HVAC.456, PSHVAC456

Download

English - pdf (130 KB)

Select Language

Victualic