Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

GS Retail

Located in Anyang, South Korea, the GS Retail Building houses offices and retail department stores. When selecting products to be installed on the piping system, the owner required products available in up to 16" in size with a maximum working pressure of 20 bar. Ultimately, the building owner chose Victaulic couplings, fittings and valves to meet these requirements. Because the owner researched past Victaulic projects that required similar working conditions, he was assured of the quality and reliability of Victaulic. In addition, Victaulic allowed construction schedules to be compressed, resulting in cost and labor savings.

Search Terms: PS-HVAC.375, PSHVAC375, PS-HVAC-375, PS.HVAC.375

Download

English - pdf (83 KB)