Case Studies

Victaulic can be found in some of the most prestigious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

M-Net Rechenzentrum München

M-Net is a telecom provider in Germany which serves both consumers and companies by providing telephone, internet and server access. The company focuses on high security data transfer while maintaining maximum performance. In 2012, M-Net opened a new datacenter in Münich for which they tasked engineer, WBE to find a reliable and fast pipe joining method for the cooling system. WBE, who installed Victaulic in numerous projects before, insisted on using Victaulic solutions for this project, which called for high quality and installation speed, despite a hesitant contractor. In the lightwall stainless steel piping system, contractor Lausser Pilgramsberg installed stainless steel couplings and fittings up to 219mm/8" in diameter. Installing Victaulic products resulted in a decrease of 20% in installation time compared to welding. Once the installation was completed Lausser Pilgramsberg was convinced of
the reliability and speed of installation Victaulic products provide compared to alternative joining methods and decided to rely on Victaulic solutions for future projects they are working on.

Search Terms: PS-HVAC.408, PS-HVAC-408, PS.HVAC.408

Download

English - pdf (91 KB)

Select Language

Victualic