Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Merit Energy Jackson Clearfork

The 2005 construction of the Merit Energy Jackson Clearfork Waterflood included the installation of a complete Victaulic system including Style HP-70 high pressure couplings, Series 712 check valves, Series 726 ball valves and grooved end fittings. By installing the Victaulic grooved products on the steel and fiberglass reinforced oil and water handling lines, Merit Energy was able to meet the high pressure requirements of the system while also experiencing ultimate cost savings over competitive joining systems. In addition, Merit Energy worked with Victaulic Construction Piping Services to obtain water flood drawings and an advanced bill of material for the project. This ensured that the proper products were staged and available, reducing on-site handling and days required to complete the piping installation.

Download

English - pdf (100 KB)