Case Studies

Victaulic can be found in some of the most prestigious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

NUROL LIFE RESIDENCES, TURKEY

Nurol Life Residences redefine luxury by offering premium, high-end residences in Istanbul.
The engineer, Dinamik, chose welded system at the beginning of the project. However, after learning about Victaulic, the owner, Nurol Insaat, asked the contractor to immediately change the whole system from welded to grooved.

With the help of 3D modeling completed by the Victaulic Construction Piping Services team, the mechanical rooms were redesigned, and Victaulic grooved pipe joining products were installed on the heating, domestic hot water and fire protection systems.
Nurol witnessed challenges with rubber bellows and leaking wafer butterfly valves in the past. Hence, they were really impressed by the vibration-dampening qualities of the Victaulic grooved system.

The unique construction of Victaulic’s grooved coupling has vibration-dampening qualities of its own and was used in the chiller plant room and the pump rooms. Utilizing the linear movement and deflection capabilities, Victaulic's flexible grooved couplings accommodated thermal expansion and contraction and avoided the use of expansion
loops, thereby solving the problems of space constraints.

Victaulic’s grooved couplings are up to five times faster to install than alternative joining methods, allowing for an accelerated construction schedule. Moreover, Victaulic couplings are installed without the use of flame or fume, eliminating fire hazards.

Overall, the project witnessed 45% time-savings as compared to a welded system.

Download

English - pdf (152 KB)

Victualic