Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Pankyo Innovalley Cluster

Located in Seongnam, South Korea, Pankyo Techno Valley has become the Korean counterpart of Silicon Valley in the US, housing dozens of R&D and innovation companies. Among its many tenants is Innovalley Inc., a Silicon Valley-based innovation company that recently moved its South Korean office to the heart of Pankyo Techno Valley. The new 10-story office building measures over 67,000 square meters, and received the equivalent of $157 million US dollars in investments. 

To complete the installation within an accelerated construction time period of 22 months, the owner and contractor relied on Victaulic products, which allowed them to install the system two to three times faster and more efficiently than welding, resulting in cost and time savings. More importantly, the fire hazard that accompanies welding was eliminated, creating a safer job-site for the workers. The owner’s main concern, however, with the HVAC system was its ability to operate safely under a 10 bar working pressure for pipe measuring above 10" – only Victaulic couplings and fittings could meet these specifications. No other supplier could give a performance guarantee.

Search Terms: PS-HVAC.335, PSHVAC335, PS-HVAC-335, PS.HVAC.335

Download

English - pdf (125 KB)