Victaulic Introduces Series 726D Super Duplex Ball Valve with Grooved Ends
Victaulic, the world's leading manufacturer of mechanical pipe joining systems, introduces the Series 726D Super Duplex Stainless Steel Vic-Ball Valve.
Download a PDF of this release in English.
Easton, PA – Victaulic, the world's leading manufacturer of mechanical pipe joining systems, introduces the Series 726D Super Duplex Stainless Steel Vic-Ball Valve. With the ability to withstand pressures of up to 1,200 psi (8200 kPa), the Series 726D is ideal for high pressure applications in corrosive environments, such as reverse osmosis and desalination piping systems.
The Series 726D is a grooved-end, high-pressure, full-port ball valve that provides faster, easier and safer installation than flanged or butt-weld valves. The valve is connected with the Victaulic Style 489DX rigid coupling, which requires only two bolts to form a secure joint, making field assembly extremely fast. With a smaller profile than a flanged valve assembly, the Series 726D achieves significant space savings, allowing it to be installed with ease in tight spaces.
The Series 726D valve offers excellent flow characteristics and uses less energy than more restrictive types of valves. The two-piece, end-entry design features a floating ball for lower torque requirements.
A unique patent-pending composite seat design provides bubble-tight sealing ability for high- and low-pressure requirements. A stem seal cartridge enables easy stem seal replacement.
The valve features an ISO 5211 standard mounting pattern for convenient mounting of remote actuation, including a full range of power actuators.
The Series 726D is available in 2-6 inches (60-150 mm) sizes.
To learn more about the Series 726D Super Duplex Ball Valve and other valves for water systems, please visit http://www.victaulic.com
.About Victaulic
Founded in 1925, Victaulic is the world's leading producer of mechanical pipe joining systems. Headquartered in Easton, Pa., Victaulic has manufacturing and distribution facilities worldwide and employs more than 3,500 people. The company develops products for a full range of industrial, commercial and institutional piping system applications. Keep in touch with Victaulic on Facebook, Twitter or LinkedIn.