Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Anglesey Apartments

The Anglesey Apartments in Queensland, Australia is a 10 story apartment
tower in the beach front community of Redcliffe. Faced with a tight
construction schedule, the contractor required a fast, efficient and reliable
method to install the building’s wet sprinkler system. Tru-Flow Services found
its solution in Victaulic Firelock® 009H EZ rigid couplings. By eliminating the
need to disassemble the coupling before installation, 009H couplings are the
easiest and fastest way to join sprinkler system piping.

From the H-Pattern and Pump Room up through the 10th floor, Tru-Flow
Services specified Victaulic 009H couplings to be installed on the hydrant
work and risers – an installation that was originally estimated to take 1 week
to complete. Due to the ease and speed of installation, Firelock 009H EZ
rigid couplings enabled the crew to complete the system in a day and a
half – 5 times faster than the original estimate, resulting in a savings of 80%
installation time and a week in labor costs. To complete the system, Tru-Flow
chose Victaulic Style 717 Check Valves and Style 705 Butterfly Valves for a
dependable, proven fire protection system.

Download

English - pdf (80 KB)