Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Edmonton Clinic North

Edmonton Clinic North is a 570,000 sq.ft./53,000 sq.m. state-of-the-art academic teaching and administration facility for the University of Alberta.

Faced with the task of having the entire penthouse mechanical room operational in 7 months, the contractor, Lockerbie & Hole, turned to Victaulic for a total system solution that would maximize productivity. To ensure efficient piping layout and coordination, the Victaulic Construction Piping Services team designed a coordinated set of 3D models, isometric drawings and bill of materials. Using Victaulic Bag and Tag services, all products were ordered and delivered where and when needed. 

To expedite installation of the piping systems, many sections of piping were prefabricated in the contractor's shop. Victaulic Quick-Vic® couplings, featuring patented installation-ready technology, maximized productivity by ensuring fast and easy pipe connections for systems up to 8"/200mm in size. Featuring a proprietary Grade "EHP" gasket rated to 250°F/121°C, these couplings provide unmatched performance on the hot water systems. To join 14"/350mm piping, Victaulic Advanced Groove System (AGS) couplings with only two housings enabled fast, easy connections that could be visually inspected for proper assembly. Victaulic pump components, Style 155 expansion joints, TA balancing valves and the 3-piece Victaulic Koil-Kit™ for rapid coil installation were additional solutions that addressed unique facility needs.

"Without the Victaulic design team on board, and the ease of installation of Victaulic products, we could not have achieved this nearly impossible feat on time. Victaulic produced hundreds of spool drawings for this project and we had zero rework on the piping systems," commented Bill Smith, Piping Superintendent, Lockerbie & Hole.

Search Terms: PS-HVAC.355, PSHVAC335, PS-HVAC-355, PS.HVAC.355

Download

English - pdf (105 KB)