Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

Golden Ears Bridge Data Center

This data center facility, located approximately five miles from the Golden Ears Bridge, is operated by Transroute, Canada and supports the automated toll equipment for the bridge. ASD Technologies selected the Victaulic Vortex™ Fire Suppression system to protect this equipment space because it can adequately suppress fires which may start inside computer rack cabinets with minimal water damage to surrounding electrical equipment. Further, since the Victaulic Vortex system only deploys water and nitrogen, it is a 100% green system which was also a requirement for this project. Another key benefit provided by the Victaulic Vortex system is its ability to be installed as a stand-alone system, dedicated to this space only. It can operate independently of the fire safety systems for the surrounding parts of the building.

Search Terms: PS-FP.121, PSFP121, PS-FP-121, PS.FP.121

Download

English - pdf (107 KB)