Case Studies

Victaulic can be found in some of the most prestegious buildings globally. Browse through the Victaulic Case Studies to learn about the unique solutions provided by Victaulic technology and services.

Victaulic Case Studies

National Stadium Warsaw

With a seating capacity of over 58,000, the new national stadium in Warsaw will be the home of the opening match of the UEFA 2012 European Football Championship, hosted jointly in Poland and in Ukraine. Construction of the stadium began in 2008 and was completed at the end of 2011, with an official opening celebration, on February 29, 2012. The new stadium will not only function as a football stadium, but as an arena for other various sports, concerts, and conventions as well. Due to its unique oval-shaped design, constructing its potable water system proved to be challenging for engineer HTW Düsseldorf.

Specifying Victaulic grooved products offered HTW Düsseldorf a reliable solution to meet the design challenge, as well as its high quality requirements. By working with Victaulic Construction Piping Services, the teams were able
to come up with a solution for accommodating the curved design of the potable water system. The curved piping system was formed using specially engineered stainless steel elbows, ranging from 8° to 11° angles, and installing them with Victaulic flexible couplings.

Working with the Victaulic team and employing Victaulic products allowed Imtech Polska to finish the project in time for the 2012 official opening.

Search Terms: PS-HVAC.372, PSHVAC372, PS.HVAC.273, PS-HVAC-372

Download

English - pdf (97 KB)

Select Language