Victaulic’s Infrastructure Solutions Support Luce Bayou Interbasin Transfer Project

Luce Bayou Interbasin Transfer Project jobsite

Victaulic’s Infrastructure Solutions Support Luce Bayou Interbasin Transfer Project

Posted on July 28, 2020

In order to meet the anticipated demand increase while also shifting to utilizing surface water in Texas, the Luce Bayou Interbasin Transfer Project (LBITP) will transfer existing surface water rights held by the City of Houston in the Trinity River to Lake Houston in the San Jacinto basin. The LBITP is a $318 million water supply project that includes a 500 MGD pump station (located on a 90-acre parcel), approximately 3.6 miles of pipelines, setting basin and maintenance facility, 23 miles of open canals to convey the untreated water to an outfall structure at Lake Houston. One of the critical components of the Luce Bayou Interbasin Transfer Project is the pig retrieval station. The components at the pig retrieval station needed to withstand not only the forces of the day to day operations, but also accommodate the settlement presented by the terrain.

Brown & Gay Engineering, Inc. chose to utilize Victaulic system solutions, which included the Style W77 AGS Flexible Coupling and the Style W257 Dynamic Movement joint. These products provided a fully restrained system solution that met the design criteria of withstanding the forces of the day to day operations while simultaneously achieving the goal of reducing the size of the vault. By using the W257 joints, BGE, Inc. could achieve 4 inches of settlement in approximately 22 feet on this installation. Traditional methods would have required more than twice the excavation to install restraining devices, such as an M11 harness.

Additionally, the Victaulic Style W77 AGS Flexible Couplings provide a quick and easy method of entry required to access the isolation systems and the cleanout and retrieval areas. The Style W77 AGS Couplings provided the flexible solutions required for future system access in the event of routine system maintenance or untimely shutdown.

Victaulic’s mechanical capabilities provided inherent value engineering that minimized construction costs and schedules while overcoming the challenges presented by the pig retrieval station.

 

Infrastructure Projects

Read more about this project in our Infrastructure projects section of the Victaulic website where you can also view multiple photos of the Luce Bayou Interbasin Transfer project throughout the process.

Learn More

Check out more information specific to how Victaulic supports the infrastructure market, click here.

 

Related posts

Jobsite to reduce land subsidence in Texas

Grooved Piping Supports Efforts to Combat Land Subsidence

Victaulic provides solutions to Texas water treatment plants that can create significant reductions in groundwater usage & land subsidence.

Hydroelectric Power Station on Yenisei River in Russia - Victaulic offers pipe joining solutions for hydropower plants

Grooved Piping Solutions Allowing for Advancements in the Hydropower Industry

Victaulic provides solutions to hydropower plants as they evolve to meet the demand for renewable, clean, and cost-effective energy sources.

Victaulic W257 Dynamic Movement Joint Wins Pipeline Industry Guild “Utility Pipeline Technology Award”

Victaulic W257 Wins “Utility Pipeline Technology Award”

Victaulic was honored by the Pipeline Industry Guild for their innovation in the pipeline industry with the W257 Dynamic Movement Joint.