Mining Necessities: How Victaulic’s Paste Backfill Solutions Optimize Underground Operations

paste backfill solutions

Mining Necessities: How Victaulic’s Paste Backfill Solutions Optimize Underground Operations

Posted on September 24th, 2025

In the complex body of an underground mine, paste backfill systems function as vital arteries, pumping life-sustaining material to previously excavated areas. These systems circulate cemented mixtures to fill voids left by ore extraction, providing the structural support necessary for continued operations.

When these arteries perform reliably, mines operate efficiently and safely. When they fail, the entire operation can come to a dangerous — and costly — halt. Victaulic’s innovative solutions keep these essential systems flowing, extending their service life while enhancing safety for the entire mining operation.

Why Paste Backfill Matters

When miners remove ore from veins, they create voids that must be filled to maintain the mine’s structural integrity. Paste backfill systems pump cemented sand or similar materials into the empty spaces extraction leaves behind, creating stable platforms that enable miners to continue extracting ore from deeper levels.

Backfill system failures have severe consequences. Beyond the immediate safety hazards, production stoppages can cost mining operations hundreds of thousands of dollars per hour. With these systems frequently operating at pressures between 800-2,500 pounds per square inch (psi), reliability is non-negotiable.

Safety Risks in Paste Backfill Systems

Traditional paste backfill systems present several critical safety challenges:

  • Manual valve operation risks: Workers must often enter hazardous areas to operate directional valves, exposing them to high-pressure environments where component failures could be life-threatening.
  • Dangerous redirection methods: Outdated systems that require manual pipe swaps for flow redirection put workers in direct contact with pressurized systems.
  • Confined space maintenance: Regular replacement of wear components requires workers to enter confined underground spaces with limited escape routes and exposure to pressurized systems.

In many underground operations, paste backfill systems must travel through boreholes and across multiple levels, creating complex piping networks requiring frequent direction changes. Each of these transitions represents a potential point of failure, particularly when dealing with abrasive materials under high pressure. These direction changes create severe challenges as the high-velocity abrasive paste material resists changing course, creating intense localized wear at impact points, similar to how a river erodes the outer bank of a curve. The redirected flow causes momentary pressure spikes, adding stress to components, while changes in flow direction can cause heavier particles to separate and accumulate, potentially creating blockages.

Standard elbows and fittings at these points wear through much faster than straight pipe sections, becoming the system’s weakest links and requiring frequent maintenance. Most concerning are the safety hazards created when these components fail under high pressure, potentially creating dangerous high-velocity jets of abrasive material that can cause serious injury to nearby workers.

Victaulic Solutions: Enhancing Safety and Reliability

Effective paste backfill system design requires components that can reliably handle high pressure, resist abrasion and provide safe maintenance access. Safety in mining operations has three critical dimensions:

  1. Initial installation safety through proper system design and component selection.
  2. Operational safety through reliable components and remote operation capabilities.
  3. Maintenance safety through quick-connect systems that reduce exposure to hazardous conditions.

From remote-operated diverter valves to wear-resistant fittings and pressure-rated couplings, Victaulic offers solutions that work together to create paste backfill systems that address all these dimensions. The result: systems that operate more safely, improve durability and reduce total cost of ownership for mining operations.

725T Diverter Valve Technology

series 725T

Victaulic’s 725T Diverter Valve represents a significant safety advancement over manual redirection methods. Remote operation capabilities allow mine operators to actuate valves from the control room or even from the surface, eliminating the need for workers to be physically present in high-risk areas.

This automation reduces risk to miners while saving valuable time during operations. The valve’s innovative “dump” featureprevents system blockage and potential borehole loss, a critical consideration when boreholes can cost millions of dollars to drill. These valves combine compact design with remote operation capabilities, making them ideal for space-constrained underground environments.

Extended Life (XL) Elbows

When abrasive paste materials change direction, the resulting wear on standard components can lead to premature failure, often at inconvenient and dangerous times. Victaulic’s XL Elbows feature additional rubber lining that cushions abrasive media at directional changes, substantially extending component life.

The XL fitting provides a 1/4-inch rubber lining in non-lined systems (or an extra 1/4″ lining in rubber-lined systems), which cushions the media as it changes direction.

This design feature allows the backfill material to change direction without tearing apart the elbow or bend, doubling or tripling the service life compared to standard components. For mine operators, this means fewer replacements, reduced downtime and lower total cost of ownership.

High-Pressure Coupling Solutions

Victaulic offers a comprehensive pressure management system that addresses the full range of pressure requirements in paste backfill applications:

  • Style 809N High-Pressure Couplings for high-pressure applications up to 3,000 psi
    • Unlike cut and rollgroove methods that can reduce pipe wall thickness by up to 50%, the 809N system welds a ring to the pipe’s exterior surface, allowing the coupling to maintain full pipe wall thickness.
    • Ideal for the highest pressure and wear zones of a paste backfill system.
    • Particularly valuable in sand plant applications where maintaining full pipe wall thickness is crucial to extended service life.
  • Style HP-170 Rigid Coupling for intermediate pressure applications up to 1,500 psi
    • Provides enhanced safety margins on standard Schedule 40 pipe.
    • Offers 50% higher pressure rating than standard couplings (1,500 psi versus 1,000 psi) on the Schedule 40 pipe.
    • Designed for intermediate transportation zones where paste backfill systems maintain substantial pressure as they move through main travel areas before reaching mining locations.
  • Endseal Style HP-70ES High-Pressure Coupling for a complete pressure management system
    • Designed for plastic-coated and rubber-lined pipe applications.
    • Ensures system integrity throughout the pressure range up to 2,500 psi.
    • Specialized end seal design protects coated pipe systems.

Cutting Downtime, Boosting Productivity

In the high-stakes underground mining environment, system reliability translates directly to profitability. Paste backfill systems that require frequent or unplanned maintenance can severely impact production schedules and budget forecasts.

Every hour of downtime in a paste backfill system can cost mining operations hundreds of thousands of dollars in lost production. When these systems fail, not only is the immediate area affected, but the mine’s entire production schedule may be compromised.

Extended maintenance periods create cascading effects throughout the operation, while rushed maintenance to minimize downtime can introduce additional safety risks. Mining operations require solutions that not only perform reliably but can be quickly maintained when necessary.

Victaulic understands this critical relationship between system uptime and operational success. The company’s approach to paste backfill focuses not only on component durability but also on making maintenance procedures faster, safer and more predictable.

Victaulic’s Maintenance Advantages

Victaulic’s grooved coupling systems offer significant advantages during maintenance operations:

This combination of benefits means mines can perform necessary maintenance more efficiently and safely, further reducing the total cost of ownership of the backfill system.

Seamless System Integration From Pump to Discharge

Underground mining operations require paste backfill systems that function seamlessly from pumping stations to discharge points across multiple levels and through various pressure zones.

Rather than offering isolated components, Victaulic approaches paste backfill as an integrated system challenge. This holistic perspective ensures compatibility between components while addressing the unique requirements of each segment of the system, from high-pressure zones near pumping stations to lower-pressure areas at discharge points.

This system approach includes a specific pressure transition strategy:

  • 809N Coupling for the highest wear and pressure areas up to 3,000 psi.
  • HP-170 Coupling for intermediate zones up to 1,500 psi.
  • HP-70ES for appropriate pressure up to 2,500 psi
  • Standard 177N couplings for lower pressure areas (800-1,000 psi, depending on pipe size)

Victaulic provides a complete solution tailored to each zone’s specific pressure requirements. These coupling solutions form a strategic pressure management system that follows the natural pressure gradient of paste backfill operations.

Partnership that Extends Beyond Equipment

Victaulic isn’t merely a product supplier, we’re your partner in optimizing paste backfill operations. Our approach includes:

  • Local experts who understand specific mining challenges and know your operation.
  • Site visits and customized system assessments to address unique challenges.
  • Engineering support and tailored solutions for your specific pressure and wear conditions.
  • Long-term relationships focused on continuous improvement and system optimization.

When you work with Victaulic, you’re getting more than industry-leading products. You’re gaining access to a team of specialists who understand the unique challenges of underground mining operations and who can provide on-site support to address your specific needs.

Mining specialists from Victaulic become valuable components of your operation, regularly visiting sites, analyzing system performance and proactively identifying opportunities for improvement. This consultative approach has made Victaulic representatives trusted partners at mines across the country, providing expertise that extends far beyond simple product supply.

Learn more about Victaulic’s mining solutions and their applications here.

 

 

 

 

Related posts

Victaulic Sponsors Mining Competition

Victaulic Sponsors Mining Competition

Victaulic sponsored the 39th Annual International Intercollegiate Mining Games, celebrating legacy mining techniques & bringing together students.

Why We Love Miner’s Day (And You Should Too!)

Why We Love Miner’s Day (And You Should Too!)

Celebrate National Miner's Day with Victaulic by learning a little more about how products derived from mines impact our daily lives.

1st In-Line Maintenance HDPE Knife Gate Valve Takes the Cake

1st In-Line Maintenance HDPE Knife Gate Valve Takes the Cake

Chemours, owner of an environmentally-friendly mining facility, used our Series 906 Knife Gate Valve for HDPE to reduce downtime & maintenance costs.

Topics: