Don’t Get Caught with your Plants Down

Portrait of male constructor forgot to do something as blooper or failure concept isolated on white with copy space area

Don’t Get Caught with your Plants Down

Posted on October 25, 2017

Let’s start with some key industry facts. The U.S. Energy Information Administration published the generating capacity figures for 2016 by facility type:

Natural Gas = 33.8%

Coal = 30.47%

Nuclear = 19.7%

Hydroelectric = 6.5%

Keep in mind, this does not include additional renewable resources such as wind or solar. Add up those percentages and you’ve got 4.08 trillion kilowatt hours (kWh) of electricity generated at utility-scale facilities in the United States. NOTE: Utility-scale facilities are power plants with at least one megawatt of capacity. To put that into scale, one kilowatt could charge 278 cell phones. Four trillion kWh translates into 14,388,489,208.6 charges; AKA more cell phones than you can go through in 100 lifetimes since the average smartphone battery endures 300-500 charging cycles. We digress – that’s a lot of energy to supply across the nation. While most individuals remain relatively unconcerned or unaware of the life cycle management of power plants, there are a handful of individuals who eat, sleep and breathe operational excellence to extend the life and service of power generating facilities.

You’re aware of the importance of keeping up with maintenance on your car so you can (mostly) avoid any serious problems that may leave you stranded on the side of the road in the wrong part of town, right? Right. Being proactive instead of reactive can save you thousands of dollars and a massive headache.

In comparison, power plants also need to factor in scheduled maintenance cycles in order to avoid emergency shutdowns which could result in lost revenues and lost minds. This heavily impacts life cycle performance. Reactivity in the form of emergency shutdowns exposes the potential for compromised safety or quality in order to expeditiously mitigate the situation. Proactivity in the form of scheduled shutdowns can be multi-phased and can allow for operational efficiency. These efficiencies include, but are not limited to, labor costs, improved reliability and alternative means of generation during downtime.

For those of you reading this who are unfamiliar with the process, you might ask yourself, when is a good time to schedule a facility outage? Planned outages are timed around demand peaks. These peaks occur in the summer and winter when heating and cooling is in full swing. That means the individuals who are responsible for overseeing operations and maintenance are left with two seasons for upgrades; the spring and fall. These outages are extremely important to the health of the plant. While some plants are flexible in meeting peak demand, such as hydro facilities, others must plan for such intervals.  The trick is to complete said maintenance faster without compromising safety or quality.

On average, the typical shutdown can take up to two months to complete. During this time, certain protocols must be followed depending on the type of work and area of the plant.

If for some reason these maintenance intervals are prolonged a few major things could happen:

1.)    Budget becomes inaccurate. You now need to factor in additional labor costs and supplementary product or equipment costs

2.)    Loss of throughput and efficiency. Every day your plant isn’t running is lost generation and/or revenue. And if you run into peak demand seasons – forget it

3.)    Potential regulatory compliance penalties for not adhering to timeline limitations

4.)    If you can’t get the plant up and running  you may need to purchase power on the open market which costs more than it takes to generate

5.)    Reliability and availability of fuel/gas to bridge generation gaps during outages. Customer gas deliveries take priority over plant deliveries

6.)    If you can’t get delivery of the gas you’ll need to pay the difference

7.)    Increased safety risk and insurance costs to keep the workers on-site

8.)    Workers Compensation risks

9.)    Contractor change orders

10.) Risk of product delivery delays if ordering last minute

Those are some hefty obstacles to overcome if you run over schedule. Luckily, there are solutions to keep you as far away from turmoil as you can get.  Victaulic Construction Piping Services (CPS), in conjunction with grooved mechanical pipe joining systems, can reduce your project lifecycle by one half. Don’t believe us? The CPS team will provide you with time studies, BOM change outs and even weight reductions. Ignorance is no longer bliss.

The moral of the story – DON’T get caught with your plants down. It detracts from the greater good and your bottom line.

Related posts

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

This innovative piping system solution allows for faster pipe fabrication & field installation, improves safety & reduces project costs.

Grooved Pipe Joining System Design Insight from Ralph Schoch

Grooved Pipe Joining System Design Insight from Ralph Schoch

Victaulic’s own Ralph Schoch discusses how using Revit can change the way engineers design grooved piping systems & improve their projects.

Advantages of Grooved Pipe Couplings Stand the Test of Time

Advantages of Grooved Pipe Couplings Stand the Test of Time

The SS John W Brown, demonstrates Victaulic’s grooved coupling reliability as it is still fully functional 70 years later.