NASA Puts Victaulic Couplings to the Test at Launch Pad & Vibration Lab

AdobeStock_294479202 (1)

NASA Puts Victaulic Couplings to the Test at Launch Pad & Vibration Lab

Posted on September 18, 2015

You wouldn’t think Victaulic would have much in common with NASA. We design and manufacture pipe joining and fire protection systems; they build spacecraft and explore the solar system, among other things. Our products are used in everything from oil wells to municipal water treatment plants to the world’s tallest skyscrapers. NASA’s products are used from Earth to Mars…and beyond.

In actuality, we have a relationship that dates back more than 30 years. After the first space shuttle flight in 1981, NASA came to us with a problem: The blistering heat, created at liftoff, scorched the piping system designed to cool the space shuttle’s mobile launch pad. NASA needed a quick way to replace the pipes, and Victaulic grooved pipe couplings were the answer. Our relationship expanded in 2013 when we realized there’s something else the two of us have in common: dealing with vibration.

NASA scientists know a thing or two about vibration. Not only do space capsules have to withstand the massive forces of launch and re-entry, the highly sensitive hardware inside them must come through in working order. To test its equipment’s ability to dampen and withstand vibration, NASA built a specialized Vibration & Acoustics Test Facility (VATF) at the Johnson Space Center in Houston, Texas. At Victaulic, we don’t have to deal with Solid Rocket Boosters or the blast of a sonic boom, but what better place to evaluate the vibration dampening and reduction capabilities of our flexible couplings than the same facility that tests spaceships?

Handling vibration in piping systems

We know you understand the importance of accommodating vibration in mechanical systems: Pumps, chillers, and other equipment generate vibration that can put stress on system components and connections. Vibration also creates noise that’s transmitted through piping systems, driving building owners and occupants mad.

But did you know you can specify Victaulic flexible couplings to attenuate vibration? Flexible couplings also accommodate expansion, contraction, and deflection generated by thermal changes, building or ground settlement and seismic activity. The flexible coupling permits this movement while maintaining a positive, self-restrained joint. The image below depicts how the components of a flexible grooved joint dampen vibration:

Cross sections of Style 177N and W77 couplings displaying how each component of the couplings handle vibration.

“This may all be true, but I’ve been using flex connectors for years. Why change?” We’ve heard that question once or twice. On one hand, the use of unrestrained rubber as a pressure boundary in a system that otherwise has continuous metallic encasement is less than ideal. More importantly, flex connectors are maintenance items that will require eventual replacement. Victaulic couplings offer continuous metallic encasement and are designed to last the life of the system—no maintenance necessary. Oh, and the most important part: Testing at NASA’s VATF proved that flexible Victaulic couplings offer better vibration attenuation than flex connectors.

Putting couplings to the test

Built to simulate space flight and capable of generating up to 40,000 pounds of horizontal and vertical force, the shakers at NASA’s VATF lab are no slouch—but neither are Victaulic flexible couplings. We put the Style 77, Style 177, Style 177N, and Style W77 to the test in configurations of one, two, and three couplings in sizes ranging from 4 to 24” (100 to 600mm). For each size, tests were also done on pipe using double sphere rubber connectors and stainless steel braided pump connectors to compare the vibration dampening capabilities. Every assembly was filled with water and pressurized to 300 psi (20 bar), and vibration was measured at the source and after the couplings or connectors.

Style W77 four coupling configuration

The results? For every size tested, three Victaulic flexible couplings installed near the vibration source outperformed the flex connectors. You read that correctly: A method traditionally used to join pipe offers better vibration attenuation than the devices commonly specified to accommodate vibration. The figures below show the performance improvement in the test configurations of Victaulic couplings over the double sphere rubber connectors and stainless steel braided pump connectors.

Two bar graphs comparing "Three Victaulic Flexible Couplings Relative Vibration Attenuation Performance over Double Sphere Rubber Connectors" vs. Stainless Steel Braided Pump Connector

Note that these results are specific to Victaulic flexible couplings. The chemical formulation and processing techniques used in Victaulic gaskets and the proprietary design of Victaulic couplings are the keys to their vibration dampening qualities.

While most engineers will never have to design a piping system for use in zero-gravity or that can withstand being rocketed into space at 18,000 miles per hour, they will be challenged to mitigate the irritating and even harmful effects of noise and vibration—if not at the design stage, then at a much less opportune time down the road. The results of the testing at NASA’s Vibration & Acoustics Test Facility prove that Victaulic flexible couplings meet and exceed these challenges, while offering additional benefits that flexible connectors just can’t match.

To learn more, review the full vibration test report.

Related posts

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

This innovative piping system solution allows for faster pipe fabrication & field installation, improves safety & reduces project costs.

Grooved Pipe Joining System Design Insight from Ralph Schoch

Grooved Pipe Joining System Design Insight from Ralph Schoch

Victaulic’s own Ralph Schoch discusses how using Revit can change the way engineers design grooved piping systems & improve their projects.

Advantages of Grooved Pipe Couplings Stand the Test of Time

Advantages of Grooved Pipe Couplings Stand the Test of Time

The SS John W Brown, demonstrates Victaulic’s grooved coupling reliability as it is still fully functional 70 years later.