4901 Kesslersville Road Easton, PA 18040
Misaligned suspended ceilings often lead to delayed or restricted sprinkler response. A benefit of flex drops is accounting for ceiling settlement.
Materials management has been a pain point for pipe fitters in the past. Flex drops simplify the otherwise lengthy process so fitters can work faster.
Unknown obstacles on site have long prevented accurate cost estimations for fire protection systems. Get it right the first time with flex drops.
Provides change in direction supplied with Victaulic EndSeal™ (ES) grooves. Available 3D radius in 90°, 45°, 22 ½°, 11 ¼° and 6° elbows.
Victaulic’s Manuel Emmerich explains how the construction industry can contribute significantly to more sustainability. The high resource consumption and
Commercial construction projects are fraught with challenges, from site complexities and permitting to coordinating trades and executing on schedule.
Victaulic’s Marcel Ley participated in an interview where he spoke about the company’s innovative sprinkler system design. The technology
Victaulic was honored by the Pipeline Industry Guild for their innovation in the pipeline industry with the W257 Dynamic Movement Joint.