Pipe Couplings Provide Noise & Vibration Control for HVAC Systems

Picture representing how noise and vibration control for HVAC systems is achieved with grooved pipe joining technology

Pipe Couplings Provide Noise & Vibration Control for HVAC Systems

Originally posted on August 21, 2018, updated on September 13, 2019.

Yes, there is proof that pipe couplings provide noise and vibration control in HVAC systems.

More specifically, there is proof that Victaulic couplings reduce pipe noise and pipe vibration and, in fact, they do it better than some of the other more traditional equipment vibration attenuation solutions.

noise and vibration control for HVAC systems using grooved mechanical couplings, pipe vibration absorber

 

The physical properties of a flexible grooved mechanical coupling make it intuitively noise dampening.

First, the housings are made of ductile iron, which naturally absorbs sound, so a ductile iron housing acts as a pipe vibration absorber. Second, the housings are tightened around and slightly compress the gasket, but do not bottom out in the groove. This allows the gasket to act like a vibration dampener. But you asked for proof.

“…the vibration attenuation provided by three Victaulic pipe couplings…

outperformed double sphere rubber connectors and stainless steel

braided pump connectors.”

 

In 2013, Victaulic completed testing at NASA’s Vibration and Acoustic Test Facility. (VATF)

We were thrilled to learn the results of the Victaulic coupling vibration testing. The results showed that the vibration attenuation provided by three Victaulic pipe couplings, installed near the source of vibration, outperformed double sphere rubber connectors and stainless steel braided pump connectors.  These specialty connectors can be quite expensive to purchase, as well as to maintain, which is why Victaulic is excited to be able to offer our customers not just an alternative HVAC equipment noise and vibration solution but a better performing option. Customers who choose to leverage Victaulic grooved mechanical pipe joining for their mechanical piping system connections will realize all of the noise and vibration benefits without having to purchase anything special, additional, or that requires maintenance. That is how Victaulic is engineering confidence into every build.

If you’d like to go deeper into Victaulic’s Sound Attenuation Testing Results or Victaulic’s noise and vibrations control in HVAC systems white Paper, we encourage you to click the links provided.

Related posts

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

This innovative piping system solution allows for faster pipe fabrication & field installation, improves safety & reduces project costs.

Victaulic Attends the AHR Expo with New Products & Technologies

Victaulic Attends the AHR Expo with New Products & Technologies

Learn about our new grooved pipe joining products & technologies at the 2015 AHR Expo in Chicago.

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

The TA Series 7CP advances hydronic balancing with its compact size & ability to engineer high performance systems.