Benefits of Using Flex Drops: Combating Ceiling Settlement

Benefits of Vic Flex flex drops

Benefits of Using Flex Drops: Combating Ceiling Settlement

Posted on March 31, 2020

Driven by feedback from contractors on the front lines, the fire protection industry has responded to challenges in both installing hard pipe and ensuring effectiveness for the life of the system. In this series, we will investigate three main benefits of flex drops and how they solve challenges presented with hard pipe installations. First, we’ll look at flex drops and how they accommodate ceiling settlement that can arise months or years after installation.

Challenge in Hard Pipe Installations: Ceiling Settlement

Suspended ceilings cannot escape the law of gravity. Due to the pliable nature of ceiling tiles, they are prone to settlement.  These ceilings are also apt to shift after building modifications have been made such as adding lighting fixtures.

What happens when a sprinkler cannot activate because it is positioning within a ceiling that has changed over time? In a suspended ceiling application, when the tiles are exposed to settlement or structural renovations, they start to sag or move independently of where the structural deck is located. Meanwhile, hard pipe sprinklers will stay in their original placement, resulting in sprinkler misalignment. Improper sprinkler head alignment limits the exposure to the heat and airflow emanated by a fire, leaving the ceiling to act as a heat deflector that may delay or prevent the sprinkler from activating.

Benefits of Flex Drop Installations: Confidence in Sprinkler Alignment

Flex drops are the ideal solution to combat misalignment. Attached directly to the ceiling, the brackets move with the structure, maintaining the same position relative to a suspended ceiling even after settlement occurs. When the bracket attached to the suspended ceiling plane and the braided hose connected to the distribution piping can move independently of each other, correct sprinkler alignment is not an issue. One of the main benefits of flex drops, as demonstrated in the image below, is that through utilizing flex drops you allow for unobstructed airflow access and exposure to potential heat from a fire, resulting in system activation confidence.

Vic-Flex vs Threaded flex drops

Discover More Benefits of Flex Drops

What are some other benefits of using flex drops?

 

To read more about sprinkler head alignment, check out International Fire Protection Magazine or to learn more about Victaulic VicFlex™ solutions, click here.

Victaulic

Victaulic is the leading producer of mechanical pipe joining solutions. Engineered with confidence, our solutions put people to work faster, while increasing safety, ensuring reliability and maximizing efficiency.

Related posts

Fire Sprinkler Head in Balcony Ceiling- Victaulic Flexible Dry Fire Sprinklers

A “Flexible” Solution to Fire Sprinkler Safety

Victaulic’s team of expert engineers developed a flexible dry fire sprinkler that is a simpler and safer alternative to traditional dry sprinklers.

Construction engineers supervising progress of construction project

Benefits of Using Flex Drops: Simplified Materials Management

Materials management has been a pain point for pipe fitters in the past. Flex drops simplify the otherwise lengthy process so fitters can work faster.

Hyatt Seattle equipped with Victaulic VicFlex flex drop

Benefits of Using Flex Drops: Fixed Versus Variable Costs

Unknown obstacles on site have long prevented accurate cost estimations for fire protection systems. Get it right the first time with flex drops.

Recent posts

Optimizing Mine Backfill with Innovative Diverter Valve Technology

Victaulic has a proven history of optimizing mine backfill system around the world. Here is a look into our innovative diverter valve technology in...

The Spectrum Center in North Carolina, USA remained operational during water system retrofit using Victaulic products

Installation-Ready™ Technology Simplifiesy Arena’s Domestic Water System Retrofit

The Spectrum Center remained operational during its domestic water system retrofit with help from Victaulic grooved solutions.

Mining Sustainability with Victaulic Mechanical Joining

Mining Sustainability with Mechanical Joining

Achieving mining sustainability goals begins with the products selected for each system within a mine. Victaulic solutions provide a positive impact.