Booming Through the Bust

Image from the 1920's of a stack of grooved pipe and a workman taking a break - Victaulic

Booming Through the Bust

Front page of the first Victaulic maritime industry brochure.Posted on November 6, 2017

A wave of change was erupting through Western society from the dramatic social and political revolution down to the rapid industrial and technological growth. It was a time for untraditional exertion – what better time to introduce a new means of pipe joining than the roaring 20’s?

Through the lavish, unfamiliar, and extremely short-lived lifestyle of many in the early 1920s, Victaulic continued to provide joining solutions that aided in project life cycles and efficiency. Despite the abrupt situational decline, new products and solutions flooded the market and continue to do so today.

Glance into the past with the first maritime industry brochure from the originator of the groove.

 

Related posts

The SS John W. Brown- demonstrates the reliability of Victaulic grooved couplings

Advantages of Grooved Pipe Couplings Stand the Test of Time

The SS John W Brown, demonstrates Victaulic’s grooved coupling reliability as it is still fully functional 70 years later.

NASA Puts Victaulic Couplings to the Test at Launch Pad & Vibration Lab

NASA tests how Victaulic flexible couplings handle piping systems vibration. Post includes results such as dampening & reduction capabilities stats.

The SS John W. Brown- demonstrates the reliability of Victaulic grooved couplings

Victaulic Grooved Couplings Emerge Undamaged from Military-Grade Test

Victaulic highlights a white paper about mechanical pipe couplings withstanding Naval combat high impact shock loads.