4901 Kesslersville Road Easton, PA 18040
Style 807N. For use on stainless steel and galvanized carbon steel potable water piping systems only. Utilizes Grade P gasket material for improve...
Exclusively for use on thin wall stainless steel pipe which features Victaulic’s proprietary StrengThin™ 100 groove profile.
Allows piping assembly at a 90 angle from the pump, saving valuable space in the mechanical room. Available flanged connections: PN10/PN16.
Big Brothers Big Sisters of the Lehigh Valley announced a new program, “Lead Big” that hopes to up its