Victaulic Introduces the Next Generation of Foundry Protective Apparel

Foundry Worker - Victaulic Leading-edge Foundry Worker Safety Coat

Victaulic Introduces the Next Generation of Foundry Protective Apparel

Posted on May 8, 2015

In the spirit of industry-changing innovations and safety initiatives, Victaulic – the global leader in mechanical pipe joining technology – has set a new standard in protection for its manufacturing employees. By partnering with Alabama-based textile manufacturer Toray Fluorofibers and fire garment manufacturer Majestic Fire Apparel, Victaulic developed a leading-edge foundry worker safety coat, offering improved molten metal splash protection as well as enhanced comfort and breathability.

The BOGU coat – named after the Japanese word for “armor”- was first envisioned as part of Victaulic’s mission for a world-class safety organization. After a year of material tests at the University of Alabama at Birmingham, the team developed both a woven and non-woven polytetraflouroethylene (PTFE) fabric that withstands the impact of a 2800 degree Fahrenheit molten iron splash.

“Our previous foundry coat was adequate from a protection standpoint, but it was hot, the fabric did not breathe well and was difficult to launder,” said Zach Jerrold, Global EH&S Manager. “The BOGU coat provides an equal, if not slightly better, level of protection but also provides a much higher level of comfort for our employees. The feedback we have received on the coats has been very positive.”

Developed with invaluable feedback from those who understand the day-to-day working demands of the foundry industry, the coat was engineered to be up to 30 percent lighter than the industry standard aluminized Kevlar jackets. When exposed to hot seasonal temperatures and the heat from molten metal, the new Victaulic safety garment offers increased durability and functionality with its breathable vents. Additionally, the coat is machine washable without degradation – protecting its inherent fire retardant properties, unlike the formerly used garments.

“Victaulic is proud of this significant safety accomplishment. These coats will withstand the rugged foundry environment much better than the existing industry standard outer garments,” said Bill D’Amico, Victaulic Global Environment Health and Safety Director. “We will share this advancement with others in the industry in the hopes of advancing foundry safety worldwide and, more importantly, the protection of our most valuable asset – our employees.”

In November 2014, Victaulic began outfitting its Lehigh Valley manufacturing workforce with the safety coats, which are now available for purchase from Majestic Fire Apparel.

Topics:

Victaulic

Victaulic is the leading producer of mechanical pipe joining solutions. Engineered with confidence, our solutions put people to work faster, while increasing safety, ensuring reliability and maximizing efficiency.

Related posts

Victaulic StrengThin Piping System

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic StrengThin Piping System now has an updated coupling design. This innovative high-pressure piping system solution for balance-of-plant ap...

Victaulic Booth at the AHR Expo

Victaulic Heads for the 2015 AHR Expo With New Grooved Pipe Joining Products and Technologies that Lead the HVACR Industry

Visit Victaulic at the 2015 AHR Expo in Chicago. Learn about our new grooved pipe joining products & technologies including industry-leading valve ...

Victaulic Compact Hydronic Balancing Valve

Victaulic Releases Compact, Precise Hydronic Balancing Valve from IMI TA

Victaulic releases a compact precise hydronic balancing valve. The new Compact Pressure Independent Balancing & Control Valve (Compact-P) TA Series...

Recent posts

Keller Auditorium mechanical room – partnered with Victaulic for successful renovation despite tight timeline & space

Total project partnership makes 100-year-old auditorium renovation a success

Total project partnership led to a successful renovation of Keller Auditorium's mechanical room, despite tight timelines and extreme spatial constr...

2021 Desalination Plant of the Year - Keppel Marina East Desalination Plant used Victaulic Infrastructure Solutions

Keppel Marina East Desalination Plant Wins 2021 Desalination Plant of the Year

Victaulic’s grooved technology provided reliable and sustainable solutions that supported the piping systems at the KMEDP.

Hydropower Facility represents Victaulic participation at the NHA hydropower industry event

Victaulic at NHA Clean Currents

Victaulic is proud to support & participate in the advancement of hydropower. Check out Victaulic at NHA Clean Currents, a hydropower industry event.